cancel
Showing results for 
Search instead for 
Did you mean: 

Measure Individual Phase Current

JPate.7
Associate II

hello sir

I am using motor control workbench 5.4.6 and EVSPIN32F0602S3 kit. Is there any function to get individual phase ( R,Y,B) current and total average power of motor ?

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @JPate.7 

I suggest to download the new version of STM32 Motor Control SDK (X-CUBE-MCSDK6)

In the "Motor Pilot" --> tab "Registers" you have access to all variables: you can read or plot them.

The current phase are I_A e I_B (the I_C can be obtained because the sum of all three is zero) the MOTOR_POWER is the total power of motor.

If you feel a post has answered your question, please click "Accept as Solution"