cancel
Showing results for 
Search instead for 
Did you mean: 

MC 6.3 with MX6.12 - attr not supported : Dmpu

Sujoy_B
Associate II

I am trying to generate code for "STM32 Nucleo packs FOC and 6-step motor control platform for three-phase, low-voltage and low-current motor" and I keep getting errors :-
Attr not supported : Dmpu  as in attached image. 

I am using cubeMX12, I have updated Java recently and I have uninstalled and reinstalled CubeMX as well. Still no luck. Log file attached. 

mc.JPG

1 ACCEPTED SOLUTION

Accepted Solutions
amina safy
ST Employee

Hello @Sujoy_B

 

this error has been understood and will be corrected in the next version of CubeMx.

Nevertheless, a workaround can be proposed to you in order to avoid having this issue,
Please try after you have deleted the following files :

1- %HOME%\.stm32cubemx\thirdparties\pdsc\EmbeddedOffice.I-CUBE-FS-RTOS.pdsc
2- %HOME%\.stm32cubemx\thirdparties\pdsc\EmbeddedOffice.I-CUBE-FS-RTOS.1.0.1.pdsc

 

Please tell us if this solves your problem

 

Kind regards

Amina

If you agree with my answer, please accept it by clicking on 'Accept as solution'.

View solution in original post

18 REPLIES 18
captat
Associate II

I am having the same issue as well, using CubeMX version 6.11.1 and MC Workbench 6.3.0. I've tried several different combinations of MC Workbench and CubeMX versions with no success.

amina safy
ST Employee

Hello @Sujoy_B

Can you give us the version of Java you had recently installed on your PC?
Thanks in advance


Best Regards
Amina

 

If you agree with my answer, please accept it by clicking on 'Accept as solution'.

I unistalled JAVA and installed the latest version from https://www.java.com/en/
I believe it is V8 update 411. 

Do you need me to share a snapshot?

AndyChen
Associate II

Same issue here. Using old projects with unchanged settings but showing the errors.

ego
Associate II

Same to me, suddenly started showing the error.

Hi @Sujoy_B,

 

can you please give us the version of JDK you have on your PC?
ps: the path is commonly : C:\Program Files\Eclipse Adoptium

 

Thanks for your feedback

Amina

If you agree with my answer, please accept it by clicking on 'Accept as solution'.

Hi Amina Safi,

 

I don't have that JDK, I don't even know what it is...

 

Thank you and regards.

Hi amina safy,

I also encounted the same problem as the initial post mentioned.

I'm using MCWB 6.30 and CubeMX 6.10

Here it's Java installed in my PC:

java version "1.8.0_411"
Java(TM) SE Runtime Environment (build 1.8.0_411-b09)
Java HotSpot(TM) 64-Bit Server VM (build 25.411-b09, mixed mode)

 

When I used any example project in MC WorkBench, I have no problem to generate Project.

I attached the project that I created in MC WorkBench 6.3 and renamed the extension to .txt in order to attach.

So you can rename it back to .stwb6

mitch1
Associate II

I have this error too. Any luck solving it?

Im not sure what it means and i dont have Java installed.