cancel
Showing results for 
Search instead for 
Did you mean: 

Is 'ke' (coefficient of BEMF) of a stepper motor specified in Vpp, Vp or Vrms?

MBaum.7
Associate III

According to AN4144, page 14/28, the coefficient 'ke' is measured by turning the stepper and measure the phase voltage with a oscilloscope. For the coefficient 'ke' in V/Hz, which voltage normation should be used:

  • Peak-to Peak, Peak or RMS?.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello @MBaum.2gartner​,

I mean peak voltage so in your waveform 1.74 V ;)

If you feel a post has answered your question, please click "Accept as Solution"

View solution in original post

3 REPLIES 3
Cristiana SCARAMEL
ST Employee

Hello @MBaum.2gartner​,

with reference to the AN4144 section 2.1, at page 14 it is suggested a method to measure the Ke parameter. The description of the method shall refer to peak voltage.

I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".

If you feel a post has answered your question, please click "Accept as Solution"
MBaum.7
Associate III

Hello Cristina

To clarify - do you mean the Peak to Peak voltage or the voltage from Ground to Peak (half of Peak to Peak). Or to refer to the measured signal in the oscilloscope screen: 1.74 V or 3.48 V?
_legacyfs_online_stmicro_images_0693W00000bit9YQAQ.png

Hello @MBaum.2gartner​,

I mean peak voltage so in your waveform 1.74 V ;)

If you feel a post has answered your question, please click "Accept as Solution"