2023-04-26 5:24 AM
According to AN4144, page 14/28, the coefficient 'ke' is measured by turning the stepper and measure the phase voltage with a oscilloscope. For the coefficient 'ke' in V/Hz, which voltage normation should be used:
Solved! Go to Solution.
2023-04-27 1:56 AM
Hello @MBaum.2gartner,
I mean peak voltage so in your waveform 1.74 V ;)
2023-04-26 6:08 AM
Hello @MBaum.2gartner,
with reference to the AN4144 section 2.1, at page 14 it is suggested a method to measure the Ke parameter. The description of the method shall refer to peak voltage.
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
2023-04-26 7:37 AM - edited 2023-11-20 7:06 AM
Hello Cristina
To clarify - do you mean the Peak to Peak voltage or the voltage from Ground to Peak (half of Peak to Peak). Or to refer to the measured signal in the oscilloscope screen: 1.74 V or 3.48 V?
2023-04-27 1:56 AM
Hello @MBaum.2gartner,
I mean peak voltage so in your waveform 1.74 V ;)