2021-10-15 05:32 AM
I want to implement sensorless FOC with B-G431B-ESC1 Discovery kit.But i don't want to use motor profiler as it's not profiling my motor properly.
Is it possible?
2021-10-15 09:04 AM
Hello @Tejashree
Yes, it is possible.
If you start the MC-SDK and select only the B-G431-ESC1 inverter, it will select by default a generic low voltage motor. You will be able to change the parameters afterwards in the Motor Parameters window.
Regards
Cedric