2023-01-27 2:26 AM
2023-01-31 1:29 AM
Hello @SBrah.1 and welcome to the ST Community.
Are you using the STM32 Motor Control Software Development Kit X-CUBE-MCSDK?
If so, what version?
Could you share more details on your application?
According to these hardware and firmware settings you can check the OC threshold set and verify if the over current protection is properly triggered by application.
2023-04-26 8:27 AM
Were you able to figure out the problem? I'm having the same issue.
2024-02-08 1:08 AM - edited 2024-02-08 1:09 AM
i have the same problem while using single shunt (sensorless) , motor pilot didn't even connect to the board