2020-02-06 10:36 PM
2020-02-14 06:04 AM
Hello,
This document is not available yet. However, you can use the Motor Control Workbench thanks to a small trick:
You can now connect to your application and control its motors.
This works (unless you control more than two motors, in which cas you will only be able to control the first two) because the monitor actually only uses the motor characteristics from the current project to work: the max application speed, bus voltage and power mainly...
Regards,
Fred V.
2020-02-14 06:04 AM
Hello,
This document is not available yet. However, you can use the Motor Control Workbench thanks to a small trick:
You can now connect to your application and control its motors.
This works (unless you control more than two motors, in which cas you will only be able to control the first two) because the monitor actually only uses the motor characteristics from the current project to work: the max application speed, bus voltage and power mainly...
Regards,
Fred V.