Hello @DMeie.2 ,
Indeed, there is an error in the implementation that do not conform to the specification. The Workbench and the Board Manager mandate that the busVoltageDivider property be defined both at feature and at hardware variant level. Bot...
Hello @DMeie.2 ,
Thanks a lot for the report. This is indeed a typo. One should read 0 and not null. The documentation will be fixed.
Best Regards,
FredV.
Hello @Nate-S ,You can start with an STM32G431VET if you prefer so (supported by the workbench). The thing is that STM32F401 only has one ADC while STM32429 has three. So the workbench will produce a project that only uses one ADC while you would get...
Hello,No, TIM4 is not stopped at this time. You can easily see that by using a debugger and setting a live view on the ENCODER_M1 structure or on the register bank of the timer. When the motor is stopped (after having run), you can turn the shaft wit...
Hello,
You can use the workbench as @SRedd.5 suggested to get a 6-Step with Hall sensors project.
However, the workbench does not support TIM20 for the time being and will only propose TIM1 or TIM8 (acutally only TIM1 in the case of the P-NUCLEO-I...