2025-01-06 07:30 AM
Hey I was I wondering if it was possible to use the x-nucleo-ihm08m1 on an 144 board.I only have 144 pin boards but couldnt find my board on MC Workbench.I also tried the motor pilot software and it said to configure the board.I suppose I can use it but without the MCWorkbench,am I correct?
2025-01-07 08:30 AM
Hello @DiogoPedrosa,
It is possible to connect a Nucleo-144 board to x-nucleo-ihm08m1 as the NUCLEO-F7x boards available on MC Workbench.
2025-01-07 09:28 AM
Oh,im sorry,I guess was dumb and didnt found it in the workbench.Now,how can I add the nucleo-f767zi in the workbench?Ive tried to import a board in the workbench but dont know where I can find this json.
Also is there a problem to use the f756zG,I suppose they are not that different from each other.
Ive attached a photo of the board selector in the workbench and one photo of the import page.
2025-01-10 12:12 AM
Hello @DiogoPedrosa,
Unfortunately, checking documentation available through "Workbench tool">About>Documentations>Release Notes", chapter "Supported devices and boards", for the STM32F7 family only "STM32F746ZG, STM32F756ZGTx , STM32F769NI" MCU are supported by the Motor Control Workbench current implementation.