cancel
Showing results for 
Search instead for 
Did you mean: 

How to integrate the parameters setup in MC workbench with IAR workbench for STEVAL-ESC001V1?

Rkama
Associate

I am able to generate a IAR workbench workspace from MC workbench after setting all the parameters but I am stuck.I am generating a 490Hz PWM signal with 50% duty cycle but the motor doesn't rotate.Is it possible to change the PWM frequency in MC workbench? Am I making some other mistake?

2 REPLIES 2

Hi,

sorry for this huge delay.

Do you have solved the issue mentioned ? Please upgrade the SW with X-CUBE-MCSDK and for PWM management please visit the section " Drone Zone" in this forum.

BR

Giuseppe Scuderi

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards