2018-10-16 12:09 AM
I am able to generate a IAR workbench workspace from MC workbench after setting all the parameters but I am stuck.I am generating a 490Hz PWM signal with 50% duty cycle but the motor doesn't rotate.Is it possible to change the PWM frequency in MC workbench? Am I making some other mistake?
2019-04-05 1:15 AM
Hi,
sorry for this huge delay.
Do you have solved the issue mentioned ? Please upgrade the SW with X-CUBE-MCSDK and for PWM management please visit the section " Drone Zone" in this forum.
BR
Giuseppe Scuderi
2021-06-22 2:11 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards