cancel
Showing results for 
Search instead for 
Did you mean: 

hi i'm using an ihmi16m1 board with a f302rb board, the problem i don't understand that the motor doesn't move nor activates. i tried to use a worbenk motor control, also to use X-CUBE-SPN16 ..... I use a 12v power supply thank you

SDall
Associate II
10 REPLIES 10

Hi @SDall​,

the X-CUBE-SPN16 is not recommended for new design.

As above mentioned the suggested SW to your project is the STM32 Motor Control SDK (X-CUBE-MCSDK-Y).

Since the conditions have changed compared to the original question I suggest you open a new thread in the dedicated STM32 Motor Control community

Remember to provide all the necessary information (HW, SW, FW version, setting and so on).

If you feel a post has answered your question, please click "Accept as Solution"