cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, World! I am using the NUCLEO F446RE and X-NUCLEO-IHM08M1 - 3 ch to create a driver for a permanent magnet motor. Error during project generation! I need help!

AndrewSibiryack
Associate III

in the attachment to the letter I attach three files, two of which are log files and one with screenshots

2 REPLIES 2
cedric H
ST Employee

Hello @AndrewSibiryack​ ,

Could you try to open the IOC file generated in your project folder directly by cubeMX tool and try to generate from there.

Let me know if it does the job.

Regards

Cedric

AndrewSibiryack
Associate III

Hi!

Thanks! Everything worked out!

Now there is an error when compiling to KEIL. it is not clear where the value of SPEED_LOOP_FREQUENCY_HZ is defined.