cancel
Showing results for 
Search instead for 
Did you mean: 

Error: "Port Open and try to configure the board" for B-G431B- ES1 hardware

Ajosh.1
Associate

I am using a B-G431B- ES1 hardware but when opening the motor pilot i am getting error : Port Open.

Also checked the COM port and it is correct ,even updated the drivers as well

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hi @Ajosh.1​ and welcome to the ST Community.

Since your question is about STM32 MCSDK, I added the topic "STM32 Motor Control".

If you feel a post has answered your question, please click "Accept as Solution"