cancel
Showing results for 
Search instead for 
Did you mean: 

Current Sensor Reading Issue in STM32F0 Discovery Board

Karthik DM
Associate III

I'm working on BLDC Motor Controller project. I'm using STM32F030R8T6 Microcontroller (STM32F030R8T6 Discovery Board) for motor control application. The motor controller is working fine but while reading motor controller current I'm not able to read 40mV voltage (Voltage drop across shunt current sensor) in ADC. after 40mV I can read voltage. I have doubt on STM32F030 Discovery ADC accuracy.

Please suggest me how can I solve this issue and suggest any microcontroller for mid level motor controller development.

Thank You.

1 REPLY 1
Laurent Ca...
Lead II

Dear @Karthik DM​ 

Sorry for the late answer.

Do you have still this problem to solve?

And just in case, if not, do not hesitate to share the final solution you found. Thanks by advance.

Best regards

Laurent Ca...