cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in Motor Pilot V0.9.20 from ST MCW 5.Y.4.21553 Rev-up Phases Configuration?

KSzul.1
Associate III

My setup:

NUCLEO-F446RE and STEVAL-IPM15B

"ST Motor Control Workbench" "Power Stage - Current Sensing" settings:

  • Shunt resistors value: 0.04 Ohm (also on PCB, but User Manual um-2014-1500-... says 0.08 ohm, another mismatch)
  • Amplifying network gain: 2.10
  • T-rise: 1500
  • T-noise: 2000

These values are in "power_stage_parameters.h" too.

However, Motor Pilot in "Rev-up" tab, "Phases configuration" -> click "Read all", reads as follows:

  • RShunt: 0.0050 ohm
  • OPAMP Gain: 24
  • Vref: 3.3 V

That effectively lowers down current/torque about 30% in rev-up phase.

Is it a bug or a feature? Motor Pilot does not read RShunt and gain values from the firmware?

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
GMA
ST Employee

Hello,

"Read all" corresponds to full fill the "Phase configuration" table only. If you want to display the table in "Amp" format and not in "S16A" format, you have to enter manually the "Rshunt" box values in order to have a correct conversion.

Best regards.

GMA

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA