cancel
Showing results for 
Search instead for 
Did you mean: 

Board Manager documentation is out !

Zied b.
ST Employee

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enable users to configure their motor-control application and produce a software project that implements it following its hardware component features. 

Wiki Link


A new documentation will arrive soon and will detail these features: 

  • Current Sensing: three-shunt-raw-currents-differential-internal-opamp-with-external-gain-and-filtered-adc-intput-hwv 

  • ICS 

  • Phase Voltage sensing feature 

  • Driver Protection feature 

The descVersion property is equal to 4 from version 6.2.0 of the MCSDK and the "contentVersion" property is added.

For questions regarding the board manager, please respond under this post.

 

Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".
5 REPLIES 5
Gboost
Associate

Hi Zied,

good news... we appreciate configuring our custom boards more easily...

However, when we are looking on version 6.2 we don't see the window as shown in the wiki see attached.

Thanks in advance for helping us.

Kind Regards#

Guenther

here the doc window: 

Gboost_0-1697809593317.png

 

thats what we are seeing on 6.2 

Gboost_1-1697809671742.png

 

 

hi @Gboost ,
The interface changes a little, but the parameters remain the same, the same functionalities are offered to the user.
Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".
DMeie.2
Senior II

What's the ETA on descVersion 4 of the documentation?

tejas_amp
Senior

Where can i find STEVAL-ESC001V1 in MCSDK ? 

Hello @tejas_amp,

Please, do not use an old post to add a new question. 
Creating a new post prevents to sending messages to all users thread. STEVAL-ESC001V1 is available in Inverter tab.

GMA_0-1730130963263.png

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA