cancel
Showing results for 
Search instead for 
Did you mean: 

.svd file for stm32f429zit6 is missing register bit positions for APB2ENR 20,21,22,26 maybe more

Franksterb92
Senior
 
3 REPLIES 3
KDJEM.1
ST Employee

Hello @Franksterb92​ ,

Thank you for bringing this issue our attention.

I confirm the issue: The 20, 21, 22 and 26 bits filed for the RCC_APB2ENR register are missing in the STM32F429.svd file.

I reported internally.

Internal ticket number: 148087 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

also the RCC/CR bit positions 28,29 are missing too

KDJEM.1
ST Employee

Hi @Franksterb92​ ,

I confirm the issue: The 28 and 29 bits filed for the RCC_CR register are missing in the STM32F429.svd file.

This issue is already posted here.

I reported internally.

Internal ticket number: 137645 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.