2023-03-22 2:44 AM
2023-03-22 3:25 AM
Hello @Franksterb92 ,
Thank you for bringing this issue our attention.
I confirm the issue: The 20, 21, 22 and 26 bits filed for the RCC_APB2ENR register are missing in the STM32F429.svd file.
I reported internally.
Internal ticket number: 148087 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-27 1:15 AM
also the RCC/CR bit positions 28,29 are missing too
2023-03-27 2:23 AM
Hi @Franksterb92 ,
I confirm the issue: The 28 and 29 bits filed for the RCC_CR register are missing in the STM32F429.svd file.
This issue is already posted here.
I reported internally.
Internal ticket number: 137645 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.