cancel
Showing results for 
Search instead for 
Did you mean: 

X-TGFX-4.24.1 - Issue with Circle progress (circle) with radius/center position > 1000

PMerv.1
Associate II

Hello, it seems there's some bug in TGFX. I have progress bar png's (600x140) and want to use it as circle progress. When I'm debugging it with background image + progress Color (no progress img) only, it's working until I increase radius and Center position [y] over values 1000. In TGFX is all working normally, but after flash into target I can see only background image and no progress. What's wrong here ?
(the same situation is , when I use Circle and change values like start/end arc and radius over 1000...)
Thanks.
PS: in attached picture the upper bar is done by normal Image progress, which is working well, but I need some arc based progress bar....)

0 REPLIES 0