2024-04-28 6:32 AM
I encountered an issue with the "Fx_NoR_Write_Read_File" application example. Upon running the application, it consistently triggers an error that redirects control flow to the Error_Handler() function within the app_filex.c file.
Note that STM32U5G9J-DK2 is a brand new board.
Application example location:
../STM32Cube/Repository/STM32Cube_FW_U5_V1.5.0/Projects/STM32U5G9J-DK2/Applications/FileX/Fx_NoR_Write_Read_File
Entering to app_filex.c function Error_Handler() here.
nor_xspi_status = fx_media_format(&nor_xspi_flash_disk, // nor_xspi_flash_disk pointer
fx_stm32_levelx_nor_driver, // Driver entry
(VOID *)NOR_DEFAULT_DRIVER, // Device info pointer
(UCHAR *) fx_nor_xspi_media_memory, // Media buffer pointer
sizeof(fx_nor_xspi_media_memory), // Media buffer size
FX_NOR_XSPI_VOLUME_NAME, // Volume Name
FX_NOR_XSPI_NUMBER_OF_FATS, // Number of FATs
32, // Directory Entries
FX_NOR_XSPI_HIDDEN_SECTORS, // Hidden sectors
LX_STM32_XSPI_FLASH_SIZE / FX_NOR_XSPI_SECTOR_SIZE, // Total sectors
FX_NOR_XSPI_SECTOR_SIZE, // Sector size
8, // Sectors per cluster
1, // Heads
1); // Sectors per track
/* Check the format nor_xspi_status */
if (nor_xspi_status != FX_SUCCESS)
{
Error_Handler();
}
Could you please help me on this
Solved! Go to Solution.
2024-04-29 3:03 AM - last edited on 2024-04-30 1:50 AM by Amel NASRI
Hello,
thank you for your report,
I reproduced the problem and entered a ticket.
Edit: Internal ticket number: 180260.
2024-04-29 3:03 AM - last edited on 2024-04-30 1:50 AM by Amel NASRI
Hello,
thank you for your report,
I reproduced the problem and entered a ticket.
Edit: Internal ticket number: 180260.
2024-04-29 6:56 AM
Thanks @Mike_ST and will wait for your update.
2024-06-11 3:09 PM
I also had the same issue, wish I saw this post a few days ago. I was trying to port the solution over to my custom project with unexplained errors. Then I ran the example application and also had this same issue. @Mike_ST do you know when an update will be coming?
Thanks.
2024-06-12 1:35 AM
Hello,
From what I can see, the fix is expected in software package version 1.7.0.
The current version available is 1.5.0.
I'm not able to tell when, as I don't have the planning.