cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L496ZGT6PU STLINK UART communication not working

RiccardoMilici
Associate

Goodmorning

I have a new STM32L496ZGT6PU board and I'm currently trying to print a message on the debugger serial terminal, I've followed many official guides step by step failing every time.

In particular, I perform the following:

  1. Connect the board through a USB type micro-B cable to my laptop (USB PWR connector).
  2. Create a new STM32 project, selecting the NUCLEO-L496ZG-P board from the board selector -> target language C++ -> initialize the peripherals with their default mode (YES).
  3. In Pinout & Configuration I go to Connectivity -> USART2 -> Mode Asynchronous and leave the default values.
  4. Device Configuration Tool Code Generation
  5. In Src/main.c simply write the following two lines of code in the main() function:

 

/* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
	  HAL_UART_Transmit(&huart2, (uint8_t*)"Ciao ", 6, 100);
	  HAL_Delay(1000);
  }
  /* USER CODE END 3 */

 

Then I build the project and start Debug keeping the default settings.

During the debug I create a new command shell console with

  • Connection Type: Serial Port
  • Serial port: COM6 (my PC seems to correctly recognize the STLINK on this COM port)
  • Baudrate: 115200
  • Data size: 8
  • Parity: none
  • Stop bits: 1

By clicking on "resume", the code seems to run, but nothing pops on the serial console.

 I tried to use an equal board, change the cable, and change USART interface but this didn't solve the problem.

1 ACCEPTED SOLUTION

Accepted Solutions

@RiccardoMilici wrote:

3. In Pinout & Configuration I go to Connectivity -> USART2 -> Mode Asynchronous and leave the default values.


User manual says it's LPUART1 connected to the VCP:

AndrewNeil_0-1732102274040.png

https://www.st.com/resource/en/user_manual/um2179-stm32-nucleo144-boards-mb1312-stmicroelectronics.pdf#page=26

View solution in original post

5 REPLIES 5
Imen.D
ST Employee

Hello @RiccardoMilici ,

Check your pins configuration and I recommend you follow these articles :

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

@RiccardoMilici wrote:

3. In Pinout & Configuration I go to Connectivity -> USART2 -> Mode Asynchronous and leave the default values.


User manual says it's LPUART1 connected to the VCP:

AndrewNeil_0-1732102274040.png

https://www.st.com/resource/en/user_manual/um2179-stm32-nucleo144-boards-mb1312-stmicroelectronics.pdf#page=26

SofLit
ST Employee

Hello, 

Simply because USART2 is not connected to STLINK virtual comport on NUCLEO-L496ZG-P board.

Based on the board schematics, you need to use LPUART1 instead:

SofLit_0-1732103560137.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@Imen.D wrote:

Check your pins configuration and the USART2 alternate functions on which pins are mapped.


It's LPUART1 - not USART2

 


@Imen.D wrote:

I recommend you follow these articles :


Yes, but they should be done in the opposite order:

 

 

You are right, I didn't pay attention on the used board.

Thank you @Andrew Neil for pointing out to me.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen