2024-11-28 01:46 PM
Hi ST Community,
I am working on a project using the STM32H723 MCU and the KSZ8863 Ethernet switch. I initially encountered issues while using a modified TCP echo server example, but after reverting to the unmodified example, the same issue persists. Communication is functional, but the system eventually crashes with the following assertion:
Assertion "mem_free: illegal memory: non-linked: double free" failed at line 661 in ../Middlewares/Third_Party/LwIP/src/core/mem.c
Here are the configurations:
Cortex M7:
Ethernet:
LwIP:
Thanks in advance for any guidance!
Best regards,
Russel Mahmud