2021-01-09 6:31 AM
Hi,
I would like using SD card with FATFS and read/write to SD card.
If i have bare-metal FW without DMA template enable it is work.
But if I enable DMA template f_mount, f_open return FR_OK but f_write, f_read Disc_error.
I setted in CubeMX SDMMC1- SD 1bit.
In DMA window added shared DMA channel (RX/TX SDMMC)
In Fatfs enabled dma template.
But doesnt work.
If in FatFS disable dma template, read/write is work propertly.
I using STM32L496RG
CubeMX 6.1.1
FW package 1.16.0
Please help.
thank you
Solved! Go to Solution.
2021-01-10 4:37 AM
I have found the solution to this problem:
2 way (RX,TX) dma doesnt work, I dont known why...
But shared DMA channel yes but in BSP_driver_cd.c CubeMX doesnt generate propertly Write *** Read function.
in file bsp_driver_sd.c in function modify BSP_SD_WriteBlocks_DMA(...):
__weak uint8_t BSP_SD_WriteBlocks_DMA(uint32_t *pData, uint32_t WriteAddr, uint32_t NumOfBlocks)
{
uint8_t sd_state = MSD_OK;
// Since we are only using 1 DMA channel for SDMMC
// Change DMA direction before calling SD Read
// Direction can only be changed when DMA is disabled
__HAL_DMA_DISABLE(hsd1.hdmatx);
hsd1.hdmatx->Init.Direction = DMA_MEMORY_TO_PERIPH;
hsd1.hdmatx->Instance->CCR |= (uint32_t)DMA_CCR_DIR;
/* Write block(s) in DMA transfer mode */
if (HAL_SD_WriteBlocks_DMA(&hsd1, (uint8_t *)pData, WriteAddr, NumOfBlocks) != HAL_OK)
{
sd_state = MSD_ERROR;
}
return sd_state;
}
in file bsp_driver_sd.c in function modify BSP_SD_ReadBlocks_DMA(...):
__weak uint8_t BSP_SD_ReadBlocks_DMA(uint32_t *pData, uint32_t ReadAddr, uint32_t NumOfBlocks)
{
uint8_t sd_state = MSD_OK;
// Since we are only using 1 DMA channel for SDMMC
// Change DMA direction before calling SD Read
// Direction can only be changed when DMA is disabled
__HAL_DMA_DISABLE(hsd1.hdmarx);
hsd1.hdmarx->Init.Direction = DMA_PERIPH_TO_MEMORY;
hsd1.hdmarx->Instance->CCR &= ~DMA_CCR_DIR;
/* Read block(s) in DMA transfer mode */
if (HAL_SD_ReadBlocks_DMA(&hsd1, (uint8_t *)pData, ReadAddr, NumOfBlocks) != HAL_OK)
{
sd_state = MSD_ERROR;
}
return sd_state;
}
Solution first posted superspud9 on reddit.
thanks
2021-01-10 4:37 AM
I have found the solution to this problem:
2 way (RX,TX) dma doesnt work, I dont known why...
But shared DMA channel yes but in BSP_driver_cd.c CubeMX doesnt generate propertly Write *** Read function.
in file bsp_driver_sd.c in function modify BSP_SD_WriteBlocks_DMA(...):
__weak uint8_t BSP_SD_WriteBlocks_DMA(uint32_t *pData, uint32_t WriteAddr, uint32_t NumOfBlocks)
{
uint8_t sd_state = MSD_OK;
// Since we are only using 1 DMA channel for SDMMC
// Change DMA direction before calling SD Read
// Direction can only be changed when DMA is disabled
__HAL_DMA_DISABLE(hsd1.hdmatx);
hsd1.hdmatx->Init.Direction = DMA_MEMORY_TO_PERIPH;
hsd1.hdmatx->Instance->CCR |= (uint32_t)DMA_CCR_DIR;
/* Write block(s) in DMA transfer mode */
if (HAL_SD_WriteBlocks_DMA(&hsd1, (uint8_t *)pData, WriteAddr, NumOfBlocks) != HAL_OK)
{
sd_state = MSD_ERROR;
}
return sd_state;
}
in file bsp_driver_sd.c in function modify BSP_SD_ReadBlocks_DMA(...):
__weak uint8_t BSP_SD_ReadBlocks_DMA(uint32_t *pData, uint32_t ReadAddr, uint32_t NumOfBlocks)
{
uint8_t sd_state = MSD_OK;
// Since we are only using 1 DMA channel for SDMMC
// Change DMA direction before calling SD Read
// Direction can only be changed when DMA is disabled
__HAL_DMA_DISABLE(hsd1.hdmarx);
hsd1.hdmarx->Init.Direction = DMA_PERIPH_TO_MEMORY;
hsd1.hdmarx->Instance->CCR &= ~DMA_CCR_DIR;
/* Read block(s) in DMA transfer mode */
if (HAL_SD_ReadBlocks_DMA(&hsd1, (uint8_t *)pData, ReadAddr, NumOfBlocks) != HAL_OK)
{
sd_state = MSD_ERROR;
}
return sd_state;
}
Solution first posted superspud9 on reddit.
thanks
2023-12-03 10:52 PM
This is great info. I don't know how we are supposed to find this out.
Anyway, FWIW, since the functions in bsp_driver_sd.c are defined as weak, you can define them anywhere in your code that is called and it will override the implementations in bsp_driver_sd.c. That way you can avoid having to replace the code each time it is auto-generated.