cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753 PING STOPPED

Ocebe.1
Associate III

Hello, I am working on Ethernet with the STM32H753 board. After configuring the necessary Ethernet settings, I can ping the assigned IP address of the board. However, after a few minutes, I can no longer ping it. What could be the reason for this issue?

I am using STM32CubeIDE version 1.17.0 and library version 1.12.0.

Thank you for your help!

2 REPLIES 2
mbarg.1
Senior II

You must share the project or we can just bet on some possible cause - like: you are not releasing packets and you run out of resources - but could be onything else

So what debugging have you done to find what's happening?

Put some diagnostics into your code so that you can see what's going on.

As @mbarg.1 said, you've given nothing to go on - but anything which stops working "after a while" smells of resources being used but not released when done ...

 

How to write your question to maximize your chances to find a solution