cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0x1 USB?

https://www.st.com/en/microcontrollers/stm32g0-series.html?icmp=tt9016_gl_****_dec2018&querycriteria=productId=SS1960 :

0690X000006CkQNQA0.png

but on https://www.st.com/content/st_com/en/products/microcontrollers/stm32-32-bit-arm-cortex-mcus/stm32-mainstream-mcus/stm32g0-series/stm32g0x1.html?querycriteria=productId=LN2048 there is no mention of USB HOST/DEV, not even in the future products.

Is this some oversight, or are 'G0x3 with USB planned?

JW

PS. Can that picture on website be provided in higher resolution, please?

14 REPLIES 14
JDUMA
Associate II

here an extract of the STM32G431x Datasheet. BR, JP​

@JDUMA​ ,

I am not talking about PD, it's completely separate from the USB data transfer.

What I am talking about is the USB "data" module. In G4, it is Device only:

0690X00000As4VGQAZ.png

but look at the initial post here, it says DEV/HOST, indicating, that G0 might have a USB module capable of being either USB Device or USB Host.

Is this the case, or is that picture a blunder?

JW

JDUMA
Associate II

​Yes that's correct (as this is shown in the portfolio overview), new STM32G0Cx are planned by next year with a USB device / host comm interface. Switching from device to host or vice versa will be possible by using "data swap" command encapsulated in the USB PD protocol. BR, JP

@JDUMA​ 

Ah, I see, thanks.

And, the second part of my question, is then that device/host module be the Synopsys OTG as used already in 'F4/'higher-end L4/'F7/'H7 (probably in its newer version), or something else?

Thanks,

Jan

Thank you