2024-05-22 12:49 AM
Hi
I successfully got the USB DFU bootlader working in 2 hours.
This one: https://www.youtube.com/watch?v=n_LDXOQHerU
Now i would like to add some encryption to it with a time budget of couple of hours.
I am already using python for USB DFU update.
What is the quickest way forward?
thx
2024-06-18 8:01 AM - edited 2024-06-18 8:02 AM
Hello @MK..1
Here's a step-by-step guide to get you started:
Step 1: Choose an Encryption Algorithm
Step 2: Install a Python Encryption Library
You can use the pycryptodome library, which is a self-contained Python package of low-level cryptographic primitives. Install it using pip:
pip install pycryptodome
Step 3: Encrypt the firmware
Before sending the firmware via DFU, you'll need to encrypt it.
Step 4: Decrypt the firmware in the bootloader
Your bootloader will need to decrypt the firmware before applying the update. You'll need to securely transfer the encryption key and IV (Initialization Vector) to the bootloader. The decryption process will be the inverse of the encryption process.
Step 5: Update the DFU script
Modify your existing Python DFU script to encrypt the firmware before sending it to the device.