2018-12-03 12:39 AM
In the file stm32l4_hal_sd.c in functions:
No check is performed on tempbuff's bounds: its value must not exceeds pData base address + pData size but tempbuff gets incremented indefinitely until a hardfault is triggered by dereferencing reserved address space.
Fix: enclose the block where tempbuff is incremented with the following condition:
if( (tempbuff - pData) < (NumberOfBlocks * BLOCKSIZE))
Solved! Go to Solution.
2020-03-25 1:12 AM
Hello @phlf ,
Please note that the fix was deployed in STM32CubeL4 V1.14 (current one is 1.15.1).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-01-23 9:02 AM
Hi @phlf ,
We recognize this issue for HAL_SD_WriteBlocks and HAL_MMC_WriteBlocks, but I am not sure that it is applicable for HAL_SD_ReadBlocks.
There is already a planning to fix it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-05-13 6:25 AM
** DELETED **
2020-03-25 1:12 AM
Hello @phlf ,
Please note that the fix was deployed in STM32CubeL4 V1.14 (current one is 1.15.1).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.