cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G4 HAL manual doesn't cover the I2S API.

Takemasa
Associate III

Hi ST support

The "Description of STM32G4 HAL and low-layer drivers" ( UM2570 rev 1.0) doesn't cover any I2S HAL API ( HAL_I2S_* ).

The manual can be downloaded from here :

https://www.st.com/ja/embedded-software/stm32cubeg4.html#resource

Please check and correct.

Takemasa

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Piranha
Chief II

This type of reports should be tagged as "Documentation", not "Bug-Report". =)

Takemasa
Associate III

Thanks, I changed!

Amel NASRI
ST Employee

Hi @Takemasa​ ,

Even with a delay, this is raised internally to add I2S HAL APIs to UM2570. Thanks for reporting.

Meanwhile, you can refer to the chm file where all APIs are defined (STM32Cube_FW_G4_V1.2.0\Drivers\STM32G4xx_HAL_Driver\STM32G474xx_User_Manual.chm and STM32Cube_FW_G4_V1.2.0\Drivers\STM32G4xx_HAL_Driver\STM32G431xx_User_Manual.chm).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.