Problems with osMessageQueue
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-21 11:39 PM - edited ‎2024-03-25 8:28 PM
Hello.
I'm using the STM32U5A9J-DK development board to work on a project to display UART data on the screen textArea, and I've made sure that there are no problems with the communication between the PC and the STM32 UART, and with the process of Model-Presender-View displaying the data on the screen.
program flow:
UART signal from PC -> main.c program receives it and saves it to CMSIS queue, get the content of queue from Model.cpp -> pass string through ModelListener.
Here is my code:
main.c
char RxData[257]; // received data from UART
char Data[257]; // copy from RxData
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
RxData[Size] = '\0';
strncpy(Data, RxData, Size+1);
if (osMessageQueueGetSpace(uartQueueHandle)>0)
{
osMessageQueuePut(uartQueueHandle, Data, 0 ,0);
HAL_UART_Transmit(&huart1, (Data), Size+1, 10); // print Data array
}
HAL_UARTEx_ReceiveToIdle_IT(&huart1, RxData, 256);
}
After "Data" is put into the Queue, I transmit to PC for display, and then I can receive the full string.
Model.cpp
char String[257];
//char data[257] = "Hello";
void Model::tick()
{
if (osMessageQueueGetCount(uartQueueHandle)>0)
{
if(osMessageQueueGet(uartQueueHandle, String, 0, 0) == osOK)
{
strncpy(RData, String, sizeof(String));
modelListener -> uart_Data(RData);
}
}
}
When I use "String" to receive, then copy it to RData and send it to View to display, the screen will display only 1~2 characters.
Another test I did was to replace "String" with the contents of data[256]. the text was displayed in full without going through the Queue.
I suspect it's a queue problem. Is there any way to display the content stored in the queue?
Here is my Queue setting, and my CubeIDE version is 1.15.0.
uartQueueHandle = osMessageQueueNew (2, sizeof(uint8_t), &uartQueue_attributes);
- Labels:
-
FreeRTOS
-
STM32Cube MCU Packages
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-22 12:38 AM - edited ‎2024-03-22 12:44 AM
Hello,
When you created your message queue how much size you configured for it?
PS: I suppose you solved your issue with UART in this thread.
So please close that thread by clicking on "Accept as Solution" on the reply which solved your issue or answered your question. Otherwise share your solution and close it by accepting it by clicking the same button.
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-22 12:47 AM - edited ‎2024-03-22 12:49 AM
@mÆŽALLEm Thanks for your reply.
This is my queue setting
------
About the previous thread
Yes, the UART communication issue has been resolved. But the struct access problem still exists.
And I'll share the UART solution for this development board later.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-22 12:53 AM
Your Queue size is 2.Increase it to the length of your string.
Item size need to be uint8_t as you are sending characters.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-22 12:56 AM
@mÆŽALLEm I've tried to change it to uint8_t in cubeMX, but it automatically changes to uint16_t
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-22 1:00 AM - edited ‎2024-03-22 3:09 AM
Change the Queue size to your string length.
For item size see this thread. Are you using cubemx 6.11?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-22 1:07 AM
I've tried to change the Queue size to 10, but nothing is changed.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-22 1:32 AM
Hello,
You need to debug your issue by creating a simple project (as done in the other thread for UART) with only FreeRTOS having two tasks one sending messages and the second receiving it and find where it fails.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-24 11:50 PM - edited ‎2024-03-25 12:29 AM
Hi, @mÆŽALLEm. the problem with the queue receiving incomplete messages is still there, but after I updated Cube MX, I was indeed able to change the data type to uint8_t.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-25 12:28 AM - edited ‎2024-03-25 12:30 AM
I would like to ask if it is possible to see the contents of the queue in debugger mode?