2022-05-26 7:08 AM
Hi,
I'm evaluating the WIFI/BLE module 1LV by Murata with a STM32H747-Dicovery board and Murata adapter as reported in the PDF file in https://github.com/Infineon/stm32-connectivity/tree/master/Documentation
The connection works fine (wifi scan OK and connection OK) and now I'm trying to increase the communication performance; the first test, using LWIP stack as server on MCU and ipref client on windows/linux side gave me only 0.15-0.20MB/s (150kBps) that seems to me very VERY slow using SDIO interface (with 25MHz clock).
Do anybody have any clues to increase this bitrate?
What can I change from the test project (https://github.com/Infineon/stm32-connectivity/tree/master/Projects/STM32H747I-DISCO/Applications/wifi_scan) to increase WIFI performance?
Do you also think that LWIP stack is the correct "library" to have good performance (at least 2.5-3.0MB/s)
Thanks
2022-05-27 2:34 AM
I'd start here:
2022-05-27 2:43 AM
another point, commercial version TCP/IP stack may have better performance.
But you have to correctly use it. otherwise you will get similar throughput.
2022-05-27 2:43 AM
Ok. Thanks
2022-05-27 2:50 AM
Ha ha - very true!
One would expect a paid-for stack to have professional support to help you with this.
Be sure to test this out as part of any evaluation...
2023-03-05 10:09 AM
For everyone, who ever reads this topic... lwIP as a stack library has no problems of pulling speeds up to: