2025-07-11 6:56 AM
When we want to debug only the M7 core, we use the following line and connect from VsCode:
/c/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.2.200.202505060755/tools/bin/ST-LINK_gdbserver.exe -cp '/c/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.2.200.202503041107/tools/bin/' -d -e -v -m 0 -gBut the problem is that always the whole processor is reset because of the following as described in
-g, --attach
Attaches to the running target.
Attach is aimed to be used to connect to a running program in the device without doing a reset or
downloading a new program.
[STM32_Programmer_CLI is always started with “mode=UR reset=hwRst” so that a device reset is
done when loading a new program independent of this option. This guarantees that the flashing of the
device is made correctly.]In our configuration the M7 is off after power on (BCM7 unchecked).
And the M4 is our main processor which starts the M7 afterwards.
When we then want to debug the M7, the whole hardware is reset and the debugger can't connect to the M7 anymore and crashes.
Is there a way to change to reset software or reset core?
2025-12-17 9:11 AM
Hello @CNien,
If the M7 is off (clock gated), it's not possible to connect to this Core. Its Access Port (AP) is 0. This is your -m 0 parameter.
But you can connect to the M4 through Access Port 3. You must change your connection parameter to -m 3.
2026-02-04 2:10 AM
Thanks for the clarification.
Our flow is the following:
After power-on, the M4 starts first and is our main core.
The M4 then enables and starts the M7.
At that point, we want to attach a debugger to the M7 (attach only, no reset).
The problem we are facing is that, even when using --attach, STM32_Programmer_CLI performs a hardware reset.
As a consequence, the whole device is reset, the M4 restarts, and the M7 is turned off again (BCM7 unchecked).
So even though the M7 was already running, the mandatory hardware reset prevents us from attaching to it and the debugger fails.
Our question is therefore:
Is there any way to avoid this hardware reset (e.g. software reset or core-only reset), or to attach to the M7 without triggering a global reset of the device?