cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to transmit and receive CAN frames using CANFD classic mode on STM32G0B1CBT3

vrushalighorpade
Associate

Hi,

I am using STM32G0B1CBT3 controller and would like to send and receive data in classic mode. I have configured all necessary parameters using cubemx but the buffer is getting full when I call this function HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData).

The CAN termination is connected properly.

Following are my configuration settings:

ClockConfig1.jpeg

clock.jpeg

FDCANClock.jpeg

CANConfig.jpeg

basicparameter.jpeg

500kbps.jpeg

0 REPLIES 0