2023-05-16 07:48 AM
Hello,
Because there are negative side effects of using FatFS in my program to write logs to an SD Card, I am trying LittleFS library with an implementation of the HAL library.
When I mount the filesystem &lfs I get a result of -84 which indicates that the fielsystem is corrupt. I made sure I tested and formatted the sd card.
I believe that my implementation of the device block operations is not complete. see attachment.
extern const struct lfs_config cfg = {
// Block device operations
.read = user_provided_block_device_read,
.prog = user_provided_block_device_prog,
.erase = user_provided_block_device_erase,
.sync = user_provided_block_device_sync,
// Block device configuration
.read_size = 16,
.prog_size = 16,
.block_size = 4096,
.block_count = 128,
.cache_size = 16,
.lookahead_size = 16,
.block_cycles = 500,
};
Help will be greatly appreciated!
2023-05-17 12:20 AM
What is LittleFS?
I also don't think this is the right place to discuss it, you may want to try to contact its authors.
JW