2018-10-11 5:10 AM
I have a 32 kHz LSE clock as output on the MCO on GPIO PA[8]. In my program I go to stop mode with wake up interrupt on several GPIOs, on of them are PC[8]. When I wake up again I don't wan't interrupt on these GPIOs and run HAL_GPIO_DeInit on them (the MCO still active). This will cause the microcontroller to get spammed with interrupts and get stuck in GPIO_EXTI_Callback.
Looking at HAL_GPIO_DeInit it contains the code:
/* Clear external interrupt configuration register */
tmp = (0x0FU) << (4U * (position & 0x03U));
CLEAR_BIT(SYSCFG->EXTICR[position >> 2U], tmp);
/* Clear EXTI line configuration */
CLEAR_BIT(EXTI->IMR, (uint32_t)iocurrent);
CLEAR_BIT(EXTI->EMR, (uint32_t)iocurrent);
/* Clear Rising Falling edge configuration */
CLEAR_BIT(EXTI->RTSR, (uint32_t)iocurrent);
CLEAR_BIT(EXTI->FTSR, (uint32_t)iocurrent);
It first clears the SYSCFG->EXTICR register before clearing the interrupt configuration. So when I run HAL_GPIO_DeInit(GPIOC,GPIO_PIN_8) it will clear the SYSCFG->EXTICR register, which when being 0 will select PA[8] as the source input for the EXTI8 external interrupt. As I still have MCO output on PA[8] this will instantly trigger interrupts and as I have rising and falling edge it will cause 64k interrupts per second. Apparently it can not handle interrupts this often as I get stuck in constant callbacks and never get to the point where the interrupt configuration is cleared.
2018-10-11 6:16 AM
Hello,
Thank you for reported this issue.
This is raised internally for check and we will come back to you as soon as possible.
Kind Regards,
Imen
2018-10-11 8:09 AM
Hello,
We confirm this issue which is already passed along to our development team for fix in the coming version of STM32CubeF0.
Thanks and Best Regards,
Imen.