2020-05-29 12:09 PM
CONTEXT:
I have been working with an STM32F429ZI Nucleo, trying to connect a USB thumb drive, to update the user application firmware. I have started with the MSC_Standalone project as it exists as an example for the F429ZI and I have been integrating relevant files from a firmware upgrade project (FWupgrade_Standalone) available for other controllers. I have not been using the Adafruit TFT shield, which the example relies on, and have removed/modified code related to it.
PROBLEM:
From my while(1) loop in main.c I'm calling the USBH_Process() function in the usbh_core.c file, and I am getting stuck with USBH_BUSY in the HOST_CLASS_REQUEST case. I followed the function calls down through the layers, and have found while debugging in the USBH_HandleControl() function (in file usbh_ctlreq.c) that the condition required (URB_Status == USBH_URB_DONE) to set the status to USBH_OK is true, yet it never enters the conditional code to set the status to USBH_OK.
URB_Status = USBH_LL_GetURBState(phost , phost->Control.pipe_out);
if (URB_Status == USBH_URB_DONE)
{
status = USBH_OK;
phost->Control.state = CTRL_COMPLETE;
...}
And so my usb host never reaches the HOST_CLASS case which I need to start any downloading function.
Does anyone know something I could try, or what I might be doing wrong?
2020-05-29 12:45 PM
> the condition required (URB_Status == USBH_URB_DONE) to set the status to USBH_OK is true, yet it never enters the conditional code to set the status to USBH_OK.
There's something rotten then. Try to single-step in disasm and observe registers/variables. Make the relevant variables volatile, recompile and observe.
JW
2021-06-02 2:57 AM
Hello.
I`m also stuck in the same USBH_Process() function, but for USB host HID. I am trying to connect a USB keyboard to my own designed stm32f407zgt6 board, code generated with STM32CubeMX v5.2.1 with package software v1.24.2 and I work with IAR IDE v8. I`ve made a project just same as (https://www.youtube.com/watch?v=Co4ChSgVSek), but with different pins pack, every time I connect the keyboard the mcu gets the descriptors, but it never gets data from keyboard. I only used one keyboard model, also searched a lot about the problem. I`ve tried what pavel.a said in (https://community.st.com/s/question/0D50X00009XkZ4KSAV/usb-host), nothing changed, when I printf() the logs on uart, at first I get:
after some "HOST_ENUMERATION"s it recognizes keyboard:
and at last the process goes on like the:
for ever "HOST_CLASS..." from USBH_Process() fuction in usbh_core.c and then "HID_GET_DATA" from USBH_HID_Process() function in usbh_hid.c.
Some place in USBH_HID_Process() function in the "HID_GET_DATA:" part of the switch_case, there is a line "HID_Handle->state = HID_POLL;", but right after this line the "HID_Handle->state" equals to "HID_GET_DATA" (see the forth picture) again very automatically.
Somebody please tell me whats going on here? I`ve also seen from my searchs that there would be a problem with boot type and request type of keyboards.
2024-03-18 3:00 AM
By HKrnr
Hi, a solution that worked in my case has been found on a similar topic. It appears the issue occurs on the row 561 of usb_ctrlreq.c, which you can replace with the following :
ep_descriptor->wMaxPacketSize |= MIN((uint16_t)(LE16(buf + 4) & 0x7FFU), (uint16_t)USBH_MAX_DATA_BUFFER);
As a new member I cannot share links, so the original topic is : FatFs_USBDisk example with USB_FS does not work. When an USB Stick is connected the USBH_MSC_Process never gets further then MSC_READ_INQUIRY. Any hints? , created by MMenz.1 on the 6th of July 2022, 2:36 AM
2024-05-22 9:09 AM
I had this problem and solved it by setting the USB clock frequency to 48MHz. In application note AN4879, section 2.4 Clock, it mentions that the USB needs a precise 48MHz clock. I looked at the clock section of the ioc interface of STM32CubeIDE and noticed the USB clock was set to 24MHz. I changed to clock settings to get 48MHz and the USB started working fine.
This might not be your problem, but it is worth taking a look at.
LK
2024-06-23 7:54 PM - edited 2024-06-23 7:57 PM
In my case, the issue of the host stuck in USBH_BUSY was solved after a small code change detailed in this ST training video (https://youtu.be/MlhUG4GsOT0?si=lECm8PH8pVmF5P4e).
Within the USBH_HID_ClassRequest function in usbh_hid.c, modify the if statement in this section of code:
FROM:
case USBH_HID_REQ_SET_PROTOCOL:
/* set protocol */
classReqStatus = USBH_HID_SetProtocol(phost, 0U);
if (classReqStatus == USBH_OK)
{
TO:
case USBH_HID_REQ_SET_PROTOCOL:
/* set protocol */
classReqStatus = USBH_HID_SetProtocol(phost, 0U);
if (classReqStatus != USBH_BUSY)
{