Skip to main content
unsigned_char_array
Lead III
December 13, 2024
Question

Hard Fault in USBH_MSC_RdWrProcess() and USBH_MSC_GetLUNInfo()

  • December 13, 2024
  • 6 replies
  • 3374 views

I have an STM32H7 and I use USB MSC. I do not use an RTOS.
If I plug in my USB thumb drive I append a counter to a file and close it.
This works.
If I remove the thumb drive very quickly at precisely the wrong moment I get a hardfault.
if Appli_state == APPLICATION_READY I set a flag and call f_open in the main loop. But then the USB drive is already gone, but there is no NULL pointer check.

We call the USBH_Process() and USBH_MSC_AppProcess() in a timer interrupt and have modified it to have non-blocking delays. I wonder if this could be the cause or if there is an actual bug in the driver that misses to check the USB drive is not available.

The following modification made to USBH_MSC_RdWrProcess() fixes the problem of hardfaults.

 

 

 

 

static USBH_StatusTypeDef USBH_MSC_RdWrProcess(USBH_HandleTypeDef *phost, uint8_t lun)
{
 USBH_StatusTypeDef error = USBH_BUSY;
 USBH_StatusTypeDef scsi_status = USBH_BUSY;

 if (phost->pActiveClass == NULL)
 {
 error = USBH_FAIL;
 return error;
 }

 MSC_HandleTypeDef *MSC_Handle = (MSC_HandleTypeDef *) phost->pActiveClass->pData;

 

 

 

 

Edit: I found an old thread that mentions the same problem:

https://community.st.com/t5/stm32-mcus-embedded-software/usb-host-library-is-not-thread-safe/m-p/307489

Another modification I made is to call an idle handler in busy waiting loops. This is not the cause of the issue, but it does address the issue mentioned by @unknown in that topic:

 

 while (USBH_MSC_RdWrProcess(phost, lun) == USBH_BUSY)
 {
 if (((phost->Timer - timeout) > (10000U * length)) || (phost->device.PortEnabled == 0U))
 {
 return USBH_FAIL;
 }
 // start of modification
 else
 {
 	// prevent blocking other processes from main context
 	usbIdleLoop();
 }
 // end of modification
 }

 

 

main:

 

void usbIdleLoop()
{
 //does non-usb things
}

int main(){
...
while(1)
{
usbIdleLoop();
usbApplication();//does fat-fs things with usb and calls usbIdleLoop in loops that were previously busy waiting to prevent blocking
}
}

 

This topic has been closed for replies.

6 replies

ST Technical Moderator
December 14, 2024

Hi @unsigned_char_array 

Thanks for reporting the issue!

Would you share an example project to reproduce on my end?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
unsigned_char_array
Lead III
December 16, 2024

That's going to be difficult, because I use a custom board. I do have a development board (STM32H735G-DK), but this one doesn't have a USB-A receptacle. I can strip the code I have right now, but pins might be different. Is that ok?
Also the problem is hard to reproduce since it requires disconnecting the thumb drive at exactly the right moment.
Maybe I can modify the code so it does more reading and writing to increase the odds of a crash.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
ST Technical Moderator
January 6, 2025

Hi @unsigned_char_array 

Would you please share your project I will check pinout and adapt your code to work with it on STM32H735G-DK board. This will greatly assist our team in diagnosing and addressing the problem more efficiently.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
cb.7
Associate III
January 16, 2025

I also have a project with STM32H7 and I use USB MSC without RTOS, I also confirm that by disconnecting a USB pen drive on the fly the system goes into hardfault and not into error. I would like to point out that I had developed my application with STM32H7 Package 1.10.0 and I had never had any problem of this type, updating to the latest 1.12.1 this bug came out. For my project it is truly a very serious error....

ST Technical Moderator
January 17, 2025

Thank you for reporting the issue @unsigned_char_array. An internal ticket is submitted to dedicated team
@cb.7 Your case on OLS is already under investigation as well. We are studying the reported behavior. 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL