cancel
Showing results for 
Search instead for 
Did you mean: 

Early Access to the STM32Cube HAL Drivers Major Update

Get early access to the next-generation STM32Cube HAL drivers for STM32U5

A major update to STM32Cube HAL drivers, called HAL2, is now available for preview on GitHub. It supports the STM32U5 series.


Building on over 10 years of experience, HAL2 delivers the following:

  • More optimized drivers with a smaller footprint and improved performance
  • Enhanced portability across STM32 devices to reduce development time
  • A more intuitive API for easier and faster application development


To support this update, examples have been revamped for better reusability and understanding, and a new online documentation portal is introduced for enhanced content and easier navigation.

Try it now:

  • Explore the preview on GitHub: STM32CubeU5-V2-Preview.
  • Test the new features and share your feedback via GitHub Issues. Your input is essential for the final release.


Join the conversation and share your thoughts in the comments.

21 REPLIES 21

@Tom_pm and @Davide Dalfra any particular series you have in mind? And is it because you are looking at starting new projects or would like to upgrade current projects? 

USBPD Dan
Associate II

To chime in re: availability on other series:

If one of the goals of HAL2 is Enhanced portability across STM32 devices, that's going to be defeated by any MCUs recently/currently in production that don't have a HAL2 framework.  Current STM HAL API is already fairly portable across processors, and in my company's codebase we make use of that.  This includes repos shared across projects.  There seem to be enough improvements in HAL2 to make an API break worthwhile, but porting STM HAL reliant code piecemeal with new processor dependencies will create desync issues between projects depending on which MCU they use.

gbm
Principal

While I generally like the changes introduced in HAL2, and especially the C startup instead of assembly, I am too dumb to understand why the ST programmers don't use bool type for simple config options and continue to use uint32_t for boolean variables. Could anybody enlighten me?

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

Hello @USBPD Dan,

 

 

Thank you very much for sharing your insights on how you and your company use HAL. Is the main challenge with the two HAL versions that HAL1 allows you to use the same application code with consistent HAL calls across multiple series, despite differences in HAL versions (e.g., STM32F7xx_HAL_Driver vs. STM32U5xx_HAL_Driver)?

If you have any suggestions on how ST could improve the experience of working with both HAL and HAL2, we would love to hear your ideas!

 

Best Regards,

Emil 

Pavel A.
Super User

Another small suggestion: calling the user callbacks in HAL code looks too verbose with #if's:

#if (USE_HAL_SD_REGISTER_CALLBACKS == 1)
      hsd->ErrorCallback(hsd);
#else
      HAL_SD_ErrorCallback(hsd);
#endif

Instead it could be defined as a wrapper  macro, for example:

     HAL_SD_INVOKE_CALLBACK(hsd, ErrorCallback); // unconditional

// where:

#if (USE_HAL_SD_REGISTER_CALLBACKS)
#define HAL_SD_INVOKE_CALLBACK(h,f) (h)->f(h)
#else
#define HAL_SD_INVOKE_CALLBACK(h,f) HAL_SD_ ## f(h)
#endif

 

I have a few practical questions regarding HAL2. I’d really appreciate official clarification:

  1. The current HAL1 library already takes up a lot of Flash space. Will HAL2 make this situation better or worse in real-world usage? Are there any reference projects or actual size comparisons between HAL1 and HAL2?

  2. Regarding RTOS and locking: Will HAL2 allow us to use an RTOS (like FreeRTOS) without forcing RTOS locks (mutexes/semaphores) on all peripherals by default?
    Real-time performance is very important to us. For example, ESP32’s ESP-IDF adds FreeRTOS mutexes to nearly every driver, and this has seriously hurt real-time capability—some high-performance tasks become almost impossible. I hope HAL2 won’t repeat this mistake and will allow us to either fully disable or customize the locking strategy.

  3. Will HAL1 continue to be maintained? Will newly released MCUs still offer HAL1 support, or will support be exclusive to HAL2 going forward?


Is the main challenge with the two HAL versions that HAL1 allows you to use the same application code with consistent HAL calls across multiple series, despite differences in HAL versions (e.g., STM32F7xx_HAL_Driver vs. STM32U5xx_HAL_Driver)?

 

That's a good summary of my concern

 


If you have any suggestions on how ST could improve the experience of working with both HAL and HAL2, we would love to hear your ideas!


 

Ideally you'll continue releasing HAL until all MCUs still in production have a HAL2 library.  Porting application code to use HAL2 isn't an issue, but having application code support both at the same time will cause undue headaches

Allow me redirect your questions to @Emil Damkjaer PETERSEN 

However...

Will HAL2 make this situation better or worse in real-world usage?

IIRC the code memory usage won't be worse because some heavy functions of HAL1 (clocks setup) have been refactored, the "MSP" functions layer removed, etc.

 Will HAL2 allow us to use an RTOS (like FreeRTOS) without forcing RTOS locks (mutexes/semaphores) on all peripherals

AFAIK, depends on the RTOS. If the RTOS supports lightweight locks similar to futex'es in Linux, then any address can act as a lock - so the lock field in the "handle" struct can legally be just a uint32_t, not any RTOS mutex or semaphore object. In C++ this kind of locks corresponds to std::atomic_t:wait() and notify_one/all().

/* Neither FreeRTOS or ThreadX have such lock, but Zephyr has */

 

Please don’t force RTOS-level locks around every peripheral call—this is a real-time killer. I think this is a very *** design, and it makes real-time tasks impossible. A lock/unlock cycle often costs orders of magnitude more CPU than the peripheral register access itself and adds jitter through rescheduling.

 

Also, many RTOS primitives (mutexes/semaphores) cannot be used from ISRs, so HAL-enforced locks clash with common ISR paths and further hurt determinism. I know this might sound harsh, but I really don’t want to see you repeat the ESP-IDF mistake.

 

Just provide a global macro or similar config to let users choose if they want real RTOS locks, or to keep the lightweight lock like in HAL1. In most cases, we don’t need locks at all—this really shouldn’t be forced by the HAL library.

TDK
Super User

HAL2 feels like a lot of spinning of wheels for little to no gain. There are a lot of good changes. I wish those changes would have been made to HAL without breaking the whole structure.

 

Random thoughts below.

 

I looked over the breaking changes pages, lots of things like this:

TDK_0-1761789012362.png

Okay, so the state enum is changing names (and possibly there is a naming convention change as well?). Who cares? This isn't an increase in functionality, just a change I have to re-learn. Doesn't decrease flash space, doesn't make anything faster, doesn't make anything clearer. It does make any existing HAL code incompatible.

 

> Split legacy HAL_PPP_Init into Init (build handle object) and config (apply configuration)

> Remove Init structure from handle and convert Init structure into configuration one

Good. Both easy hanging fruit in terms of reducing memory footprint.

 

> Add HAL User Data Set/Get APIs

> const void *HAL_TIM_GetUserData(const hal_tim_handle_t *htim)

Okay, but why make the data const? Surely "user data" should be allowed to be modified by the user. Oversight? Maybe I'm missing something.

 

> HAL implementation relies on LL inline functions instead of direct register access.

I really hate this. Now you just added another step to me figuring out what the code does. The LL functions obfuscate things, the don't help clarity.

In HAL1, I know exactly what this does after reading it:

MODIFY_REG(hdcache->Instance->CR, DCACHE_CR_CACHECMD, 0U);

In HAL2, I have no clue what this does, that it modifies the CR register, or that it modifies the CACHECMD field.

LL_DCACHE_SetCommand(p_dcachex, LL_DCACHE_COMMAND_NO_OPERATION);

 

> HAL defines and enum(those used for HW registers) are redirected to the equivalent LL ones.

Ow wow, I hate this one too. More obfuscation. And the reasoning is terrible:

> This allows for an easier transition from a HAL-based application to an LL-based application.

If I wanted to use LL, I would use LL!

 

> All public macros related to hardware (HW) are removed, and equivalent services added to the LL layer.

More marriage between HAL and LL, yuck. So they are no longer separate. HAL uses LL heavily.

 

> In HAL2, all the MspInit and MspDeInit functions are removed, including the global ones and the PPP ones. The equivalent of the global MSP Init and DeInit are respectively expected after the generated call to HAL_Init and HAL_DeInit (without using any callback). The equivalent of the peripheral MSP Init and DeInit are respectively expected after the generated call to HAL_PPP_Init and HAL_PPP_DeInit (without using a callback).

I'd like to see this. The Msp functions were confusing because it's not clear at first glance that (a) they exist and (b) get called indirectly by HAL_xxx_Init.

 

> Merge HAL extension files with common ones and remove the EX prefix from APIs

Reasonable. Should have been done a while ago.

 

> In HAL2, the lock mechanism is replaced by HAL_PPP_AcquireBus and HAL_PPP_ReleaseBus APIs that use an RTOS semaphore object.

So HAL2 forces you to use an RTOS? Huh? That's incompatible with what I do with embedded electronics, at the least.

 

> New atomic state update macro for internal HAL PPP drivers implementations (HAL_CHECK_UPDATE_STATE)

New implementation here: STM32CubeU5-V2-Preview/stm32u5xx_drivers/hal/stm32u5xx_hal_def.h at 0cf320046f0147a87c5db327c4d7e67e7b75eb27 · STMicroelectronics/STM32CubeU5-V2-Preview

I guess with LDREX/STREX we are leaving some families unable to use this and left behind with HAL2. Goodbye blue pill (good riddance). Goodbye L0, G0, and others.

 

HAL has some issues, but burning it down and trying to duplicate the library in a slightly different way is a lot of work for not much gain. This is different than standard peripheral libraries -> HAL which actually introduced fundamental differences, and overhead, into the API. Improved functionality at the cost of overhead.

 

> Removing HAL1 lock mechanism

> Adding a new HAL2 HAL OS

I generally like this, as long as it's optional, but removing it from the normal HAL2 functions means a lot of users are just not going to do it and then wonder why HAL2 isn't thread-safe.

 

> Add HAL_PPP Prefix to All HAL Peripheral APIs (Defines, Macros, Types, and Functions).

Good change.

 

 

Tried to follow some examples but I can't figure them out. Where is mx_example_tim_init?? It's not in example.c. Maybe just not done. Not a fan of the new main.c structure.

STM32CubeU5-V2-Preview/examples/hal/tim/pwm_output/application/example.c at main · STMicroelectronics/STM32CubeU5-V2-Preview

 

 

> Development toolchains and compilers

Missing is STM32CubeIDE. Are we just abandoning it entirely?

If you feel a post has answered your question, please click "Accept as Solution".