2019-04-16 1:44 AM
Hi,
I am working on board STM32L476G-DISCO, and I want build the example in STM32Cube_FW_L4_V1.13.0 Repository, ({USERNAME}\STM32Cube\Repository\STM32Cube_FW_L4_V1.13.0\Projects\32L476GDISCOVERY\Examples\BSP),
it all build successfully but at the end it show error
(compiling main.c...
linking...
STM32L476G-Discovery\STM32L476G-Discovery.axf: Warning: L6988W: Ignoring unknown patch sdcomp-29491-629360.
STM32L476G-Discovery\STM32L476G-Discovery.axf: error: L6050U: The code size of this image (33298 bytes) exceeds the maximum allowed for this version of the linker.
Finished: 0 information, 1 warning, 0 error and 1 fatal error messages.
"STM32L476G-Discovery\STM32L476G-Discovery.axf" - 1 Error(s), 1 Warning(s).
Target not created.)
How to solve this problem??????
Regards.
Rizwan
Solved! Go to Solution.
2019-04-18 8:22 AM
Hello,
Are you using MDK-ARM Evaluation Version? There is a code-size limitations (see Keil limitations)
Regards,
Imen
2019-04-18 8:22 AM
Hello,
Are you using MDK-ARM Evaluation Version? There is a code-size limitations (see Keil limitations)
Regards,
Imen
2019-04-19 3:44 AM
Yes, I am using the MDK-ARM (Keil), You are right it has limitations, when I decrease code size then this error was disappear.
Thanks
Regards
Rizwan