cancel
Showing results for 
Search instead for 
Did you mean: 

Powering the 32L476GDISCOVERY board via USB USER

NDecr.1
Associate

Hello all,

I am trying to get started with a STM32DISCO board, like described here:

https://www.st.com/en/evaluation-tools/32l476gdiscovery.html#documentation

However, I can't get it powered.

I use the USB USER connector to power it with my laptop.

SB settings 13, 15, 16 and 17 are correct.

I also can't find demo code for this board.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Powering the 32L476GDISCOVERY via external 5V_I or USB USER CN7 (USB FS connector) is mentioned in UM1879, section 10.2, page 16:

To use the USB USER CN7 to power supply the board, a jumper needs to be placed between VUSB pin 4 and the pin 3 5V_I of P2 header (see Figure 8).

The binary of the demo code is available at the website of the 32L476GDISCOVERY.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Powering the 32L476GDISCOVERY via external 5V_I or USB USER CN7 (USB FS connector) is mentioned in UM1879, section 10.2, page 16:

To use the USB USER CN7 to power supply the board, a jumper needs to be placed between VUSB pin 4 and the pin 3 5V_I of P2 header (see Figure 8).

The binary of the demo code is available at the website of the 32L476GDISCOVERY.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.