2023-08-24 11:26 AM
Hello Community , can i use X-CUBE-GNSS1 software and the X-NUCLEO-IKS01A2 expansion board together with a nucleo board to develop an application that combines both GNSS functionalities and MEMS sensors ? if yes , how can i connect them to the board , and how can i configure the pins to avoid conflicts sonce they share some pins on the nucleo F401RE board ?
2023-08-25 12:37 AM
Hello @khairi and welcome to the Community :)
The X-CUBE-GNSS1 package is the software running on X-NUCLEO-GNSS1A1 or X-NUCLEO-GNSS2A1 expansion boards. (not dedicated to X-NUCLEO-IKS01A2 expansion board)
Please have a look at this list of software for X-NUCLEO-IKS01A2 expansion board.
Imen
2023-08-26 3:17 PM
thank you @Imen.D for you reply,
maybe i wasn't clear in my request . My question was , can i combine the two sensors together on the Nucleo board ( F401RE + X-NUCLEO-GNSS1A1 + X-NUCLEO-IKS01A2) and how can i configure the pinout .
2023-08-28 10:03 AM
Hi @khairi ,
You can combine the expansion board on the Nucleo board, as the X-NUCLEO expansion board is compatible with the Arduino™ UNO R3 connector and the ST morpho connector, so it can be plugged to the STM32 Nucleo development board and stacked with additional STM32 Nucleo expansion boards.
Hope this answer your question.
Imen