cancel
Showing results for 
Search instead for 
Did you mean: 

USB OTG HS STM32F407 BOARD

Professor_Berlin
Associate II

I have successfully implemented the USB_OTG_FS as host as mass storage class on the STM32F407 discovery board. Now I want to do the same with the USB_OTG_HS 

But there is no usb connector available on the discovery board 

Can anyone guide me what external components to use and also an example code for the same. 

 

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief III

>Now I want to do the same with the USB_OTG_HS

Why ? It will/can do exactly the same as USB_OTG_FS .

 

>But there is no usb connector available on the discovery board 

Obviously ...so you have to connect a USB socket yourself.

or something like this:

https://www.reichelt.de/usb-pinheader-buchse-auf-usb-a-buchse-40-cm-delock-83825-p163112.html?&trstct=pos_8&nbc=1

 

AScha3_0-1717423350615.png

+ just solder the wires to the correct pins !

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Chief III

>Now I want to do the same with the USB_OTG_HS

Why ? It will/can do exactly the same as USB_OTG_FS .

 

>But there is no usb connector available on the discovery board 

Obviously ...so you have to connect a USB socket yourself.

or something like this:

https://www.reichelt.de/usb-pinheader-buchse-auf-usb-a-buchse-40-cm-delock-83825-p163112.html?&trstct=pos_8&nbc=1

 

AScha3_0-1717423350615.png

+ just solder the wires to the correct pins !

If you feel a post has answered your question, please click "Accept as Solution".
Muhammed Güler
Senior III

You need to use separate hardware for USB HS.
There is a tutorial below.

 

https://stm32world.com/wiki/STM32_High_Speed_USB