2024-05-14 09:11 AM
Hello everyone, i am currently working on STM32 NUCLEO-L073RZ Projects with Ardunio Ide. I did not change anything from yesterday only i install mbed studio and after installation i delete. I did not do anything with mbed just installation, and i took these errors attached with pictures. There are also Fail.txt file in Disk. How can i solve problems. All jumpers are located in correct place.
Sketch uses 8024 bytes (4%) of program storage space. Maximum is 196608 bytes.
Global variables use 868 bytes (4%) of dynamic memory, leaving 19612 bytes for local variables. Maximum is 20480 bytes.
"C:\Users\alpal\AppData\Local\Arduino15\packages\STM32\tools\STM32Tools\1.4.0/tools/win/massStorageCopy.bat" -I "C:\Users\alpal\AppData\Local\Temp\arduino\sketches\03AC7BC7F6E3ABB77F4268DAA235E17A/sketch_may14a.ino.bin" -O "NODE_L073RZ"
Insufficient disk space on current disk.
Insert another disk and type <Return> to continue...
Insufficient disk space on current disk.
Insert another disk and type <Return> to continue... Failed uploading: uploading error: exit status 2
2024-05-14 09:15 AM
And the SIZE of the .BIN is WHAT?
Can you drag-n-drop it manually?
What version of firmware is on the ST-LINK/V2-1 ? If it is old, perhaps use the update from sTM32 Cube Programmer.
2024-05-14 09:16 AM
As you're working with the Arduino IDE, and these messages are coming from the Arduino IDE, you'd be better asking on the Arduino IDE forum:
IDE v1.x: https://forum.arduino.cc/c/using-arduino/ide-1-x/18
IDE v2.x: https://forum.arduino.cc/c/software/ide-2-x/93
2024-05-14 09:16 AM
I added STM32CUBE IDE pictures i am taking another errors as you can see
2024-05-14 09:18 AM
Pardon? I don't understand!
You said you were using the Arduino IDE ?
Please clarify!
2024-05-14 09:20 AM
@alpaltunsoy wrote:There are also Fail.txt file in Disk.
So what does that file tell you?
What "disk" is it on?
2024-05-14 09:20 AM
My STLINK is updated but it does not working
2024-05-14 09:21 AM
2024-05-14 09:24 AM
I wonder if you've crashed the chip, or stuck it in low power mode
Jumper BT0 and VDD (ie BOOT0=HIGH) so that it boots the system loader rather than user space code.
See if you can connect in STM32 Cube Programmer, and then mass erase part.
2024-05-14 09:26 AM - edited 2024-05-14 09:27 AM
It think the screen shot is showing CubeIDE as unable to connect to the target. Failed file probably communicating something similar.
Check also the pair of ST-LINK jumpers on the NUCLEO, that it can connect to the TARGET.
Try the BOOT0=HIGH method I describe in the other post.
Also check current measurement jumper is connected, otherwise the TARGET will not be powered.
Check 3V3 supply at IC