cancel
Showing results for 
Search instead for 
Did you mean: 

stm32G474QET6TR pinout figure

Zachary_Chen
Associate II

Where is the stm32G474QET6TR pinout figure?

I cannot find it in the datasheet.

I need to know which pins on the board are PC3, PA11 or PB2.

like this picturepinout.PNG

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,

For this you need to refer to the datasheet of the MCU and not to the board UM.

https://www.st.com/resource/en/datasheet/stm32g474cb.pdf / Table 12. STM32G474xB/xC/xE pin definition

Figure 10:

SofLit_0-1715162251226.png

SofLit_0-1715162385509.png

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
SofLit
ST Employee

Hello,

The board's pinout description are provided in UM2505 / tables Table 15. for ARDUINO® connectors pinout and Table 16. for ST morpho connectors.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
STTwo-32
ST Employee

Hello @Zachary_Chen 

This MCU "STM32G474QET6TR" is not used in any board.  if you are tooking about the Board that you are sharing, here are the 3 Pins:

STTwo32_0-1715157353778.png

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks. I found the figure in UM2505, but the figure is for G431RB, G474RE, and G491RE.

Is the figure also suitable for "G474QET6TR"?

st-pinout.PNG

Hello,

I didn't understand!

"G474QET6TR" device is a 128 pin package:

SofLit_0-1715160475628.png

While G474RE used in the Nucleo board is a 64 pin package:

SofLit_1-1715160560957.png

So the 128 pin package is not compatible with that Nucleo board.

So could you please explain what do you want to do?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I want the pinout figure for "G474QET6TR".

I only found the "G474RE" pinout figure.

I didn't found the pinout figure for "G474QET6TR" in its datasheet.

Do you know where is the "G474QET6TR" pinout figure?

Hello,

For this you need to refer to the datasheet of the MCU and not to the board UM.

https://www.st.com/resource/en/datasheet/stm32g474cb.pdf / Table 12. STM32G474xB/xC/xE pin definition

Figure 10:

SofLit_0-1715162251226.png

SofLit_0-1715162385509.png

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.