cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProg: No STM32 target found on ST-LINK

FSkro.1
Associate II

I have a board (MCU: STM32H7B3LIH6Q) that I've been trying unsuccessfully to connect to using an external J-Link module, and recently I've switched to the internal ST-Link debugger. However, when I try to connect on STM32CubeProg for software reset, I get this output:

  16:55:24 : ST-LINK SN  : 0035002E3438510534313939
  16:55:24 : ST-LINK FW  : V3J8M3
  16:55:24 : Board       : STM32H7B3I-DK
  16:55:24 : Voltage     : 3.28V
  16:55:24 : No STM32 target found!
  16:55:24 : ST-LINK SN  : 0035002E3438510534313939
  16:55:24 : ST-LINK FW  : V3J8M3
  16:55:24 : Board       : STM32H7B3I-DK
  16:55:24 : Voltage     : 3.28V
  16:55:24 : Error: No STM32 target found!

For hardware reset, I get the following:

  16:54:40 : ST-LINK SN  : 0035002E3438510534313939
  16:54:40 : ST-LINK FW  : V3J8M3
  16:54:40 : Board       : STM32H7B3I-DK
  16:54:40 : Voltage     : 3.28V
  16:54:41 : ST-LINK error (DEV_CONNECT_ERR)
  16:54:41 : ST-LINK SN  : 0035002E3438510534313939
  16:54:41 : ST-LINK FW  : V3J8M3
  16:54:41 : Board       : STM32H7B3I-DK
  16:54:41 : Voltage     : 3.28V
  16:54:41 : Error: ST-LINK error (DEV_CONNECT_ERR)

4 REPLIES 4
Houda GHABRI
ST Employee

Hi @FSkro.1​ ,

Can you please try to connect under reset and tell me if it is Ok?

0693W00000BbW1iQAF.png 

Houda

VTaya.1
Associate III

Hi

I Have faced the same issue. Pull up boot pin of controller to 3.3v, reconnect your device with boot pin pull up. And try connecting to smt32cubeProgrammer.

It worked for me.

Under reset or in power down mode I get the following:

  09:06:08 : ST-LINK SN  : 0035002E3438510534313939
  09:06:08 : ST-LINK FW  : V3J7M2
  09:06:08 : Board       : STM32H7B3I-DK
  09:06:08 : Voltage     : 3.28V
  09:06:09 : ST-LINK error (DEV_CONNECT_ERR)
  09:06:09 : ST-LINK SN  : 0035002E3438510534313939
  09:06:09 : ST-LINK FW  : V3J7M2
  09:06:09 : Board       : STM32H7B3I-DK
  09:06:09 : Voltage     : 3.28V
  09:06:10 : Error: ST-LINK error (DEV_CONNECT_ERR)

I've been trying booting up from flash and sys mem in alternation, but both produce the same output.