2021-06-17 10:36 AM
I have a board (MCU: STM32H7B3LIH6Q) that I've been trying unsuccessfully to connect to using an external J-Link module, and recently I've switched to the internal ST-Link debugger. However, when I try to connect on STM32CubeProg for software reset, I get this output:
16:55:24 : ST-LINK SN : 0035002E3438510534313939
16:55:24 : ST-LINK FW : V3J8M3
16:55:24 : Board : STM32H7B3I-DK
16:55:24 : Voltage : 3.28V
16:55:24 : No STM32 target found!
16:55:24 : ST-LINK SN : 0035002E3438510534313939
16:55:24 : ST-LINK FW : V3J8M3
16:55:24 : Board : STM32H7B3I-DK
16:55:24 : Voltage : 3.28V
16:55:24 : Error: No STM32 target found!
For hardware reset, I get the following:
16:54:40 : ST-LINK SN : 0035002E3438510534313939
16:54:40 : ST-LINK FW : V3J8M3
16:54:40 : Board : STM32H7B3I-DK
16:54:40 : Voltage : 3.28V
16:54:41 : ST-LINK error (DEV_CONNECT_ERR)
16:54:41 : ST-LINK SN : 0035002E3438510534313939
16:54:41 : ST-LINK FW : V3J8M3
16:54:41 : Board : STM32H7B3I-DK
16:54:41 : Voltage : 3.28V
16:54:41 : Error: ST-LINK error (DEV_CONNECT_ERR)
2021-06-21 1:42 AM
Hi @FSkro.1 ,
Can you please try to connect under reset and tell me if it is Ok?
Houda
2021-06-22 5:05 AM
Hi
I Have faced the same issue. Pull up boot pin of controller to 3.3v, reconnect your device with boot pin pull up. And try connecting to smt32cubeProgrammer.
It worked for me.
2021-06-22 6:08 AM
Under reset or in power down mode I get the following:
09:06:08 : ST-LINK SN : 0035002E3438510534313939
09:06:08 : ST-LINK FW : V3J7M2
09:06:08 : Board : STM32H7B3I-DK
09:06:08 : Voltage : 3.28V
09:06:09 : ST-LINK error (DEV_CONNECT_ERR)
09:06:09 : ST-LINK SN : 0035002E3438510534313939
09:06:09 : ST-LINK FW : V3J7M2
09:06:09 : Board : STM32H7B3I-DK
09:06:09 : Voltage : 3.28V
09:06:10 : Error: ST-LINK error (DEV_CONNECT_ERR)
2021-06-22 6:53 AM
I've been trying booting up from flash and sys mem in alternation, but both produce the same output.