2023-12-11 1:08 AM
Hello,
I bought a NUCLEO-H743ZI2 board.
When I plugged it in for the first time, I was able to flash it after two or three attempts (ST-Link was often not recognised).
But now the STM32CubeProgrammer does not recognise the ST-Link at all (I have tried more than 20 times with different USB cables).
When I plug the board into the PC, I get a virtual COM port "STMicroelectronics STLink Virtual COM Port (COM23)" in the device manager.
So the ST-Link seems to communicate. But the programmer still does not recognise it.
What could be the reason?
Solved! Go to Solution.
2023-12-11 3:14 AM
This is not my Problem.
My problem was that the on-board ST-Link was not recognices.
But I found a solution: This problem only happens if I connect the NUCLEO Board via my USB hub to the Laptop.
If I connect it directly to the Laptop it works fine.
2023-12-11 1:46 AM
2023-12-11 3:14 AM
This is not my Problem.
My problem was that the on-board ST-Link was not recognices.
But I found a solution: This problem only happens if I connect the NUCLEO Board via my USB hub to the Laptop.
If I connect it directly to the Laptop it works fine.
2023-12-11 5:53 AM
Hubs and Docking Stations have historically been an issue. Gets particularly troublesome with External Loaders, and pushing 8 - 32MB of data, and the connection randomly failing mid process. Issue with board/drivers and ability to recover / retry