2024-10-25 2:11 AM
Hello, I am working on a diy simracing project which use the STM32F401CCU6 board. I just bought this board and It worked fine until today for a reason I ignore. The board is stuck on the red led, the blue led doesn't light up anymore. I can still find the board in the device manager ( picture under ) but not it is not detected as it shall be in game controller configuartor ( picture under ). I can still erase the sketch on STM32 Cubeprogrammer and upload it but when I disconnect it it stays with the red led.
Have anyone any idea on what to do ?
Thanks you for your answers, and sorry for my english which isn't very good !
Solved! Go to Solution.
2024-10-25 2:45 AM
@Totouan wrote:But does it really change something ?
It means the chip may not function correctly
@Totouan wrote:There aren't any other option than to buy a real one ? N
That would be the best route if you want to avoid a load of grief!
eg, see:
@Totouan wrote:The board is stuck on the red led, the blue led doesn't light up anymore. I can still find the board in the device manager ( picture under ) but not it is not detected as it shall be in game controller configuartor
That picture shows that it is stuck in Bootloader mode - ie, it's waiting for you to download firmware.
Because it's stuck in Bootloader mode, it won't be detected as a game controller - or anything else - until you've successfully loaded good firmware.
2024-10-25 2:16 AM - edited 2024-10-25 2:17 AM
2024-10-25 2:18 AM
I bought this STM32F401CCU6 board on aliexpress : https://fr.aliexpress.com/item/1005006127532207.html?spm=a2g0o.order_list.order_list_main.28.29545e5bxmk3BU&gatewayAdapt=glo2fra
2024-10-25 2:28 AM
So (almost) certainly not a genuine STM32
2024-10-25 2:34 AM
But does it really change something ? There aren't any other option than to buy a real one ? No idea of what to do anyway ?
2024-10-25 2:45 AM
@Totouan wrote:But does it really change something ?
It means the chip may not function correctly
@Totouan wrote:There aren't any other option than to buy a real one ? N
That would be the best route if you want to avoid a load of grief!
eg, see:
@Totouan wrote:The board is stuck on the red led, the blue led doesn't light up anymore. I can still find the board in the device manager ( picture under ) but not it is not detected as it shall be in game controller configuartor
That picture shows that it is stuck in Bootloader mode - ie, it's waiting for you to download firmware.
Because it's stuck in Bootloader mode, it won't be detected as a game controller - or anything else - until you've successfully loaded good firmware.
2024-10-25 2:48 AM
Okay thanks for your time and answer !
2024-10-25 3:06 AM
And do you have any idea of how to unstuck it from the bootloader mode ?
2024-10-25 3:11 AM
Load some code into it!
You'll have to find out what app(s) is/are required to do that.
Or use an ST-Link (or similar) to program directly.
2024-10-25 3:15 AM
Okay thanks a lot !