cancel
Showing results for 
Search instead for 
Did you mean: 

Please review the schematics designed using STM32F427VGT6.

NANTO.1
Associate II
 
5 REPLIES 5
Javier1
Principal

@NANTO.1​ is there any problem with your design at all?

we dont need to firmware by ourselves, lets talk
NANTO.1
Associate II

I didnt saw any problem. So I send schematics to you to check and confirm.

I dont think thats the correct approach to use this forum.

we dont need to firmware by ourselves, lets talk
TDK
Guru

Seems like a fine use of the forum to me. More interesting to look at than a lot of other posts.

The analog/digital grounds should be tied together and not separated by a filter. If you want to filter, do it on the positive side.

VCAP pins should be tied together per the reference manual, doubt it will be an issue.

If you feel a post has answered your question, please click "Accept as Solution".

Hello

The NRST pin is treated as input.

Note that the NRST pin may be pulled low by any of the internal reset sources of the MCU. POR , IWDG SWReset, etc