2021-04-27 10:42 PM
2021-04-27 11:44 PM
@NANTO.1 is there any problem with your design at all?
2021-04-28 12:01 AM
I didnt saw any problem. So I send schematics to you to check and confirm.
2021-04-28 1:32 AM
I dont think thats the correct approach to use this forum.
2021-04-30 9:10 AM
Seems like a fine use of the forum to me. More interesting to look at than a lot of other posts.
The analog/digital grounds should be tied together and not separated by a filter. If you want to filter, do it on the positive side.
VCAP pins should be tied together per the reference manual, doubt it will be an issue.
2021-04-30 1:37 PM
Hello
The NRST pin is treated as input.
Note that the NRST pin may be pulled low by any of the internal reset sources of the MCU. POR , IWDG SWReset, etc